AXIS#.MOTOR.IDMAX

Description

This parameter is supported for IPM motors (AXIS#.MOTOR.TYPE = 6). AXIS#.MOTOR.IDMAX is the maximum motor winding current in the direct (non-torque producing) axis.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 6

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0.2 to 1000

Default Value

0.5 * AXIS#.MOTOR.IPEAK

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.IDMAX

500bh

27h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.IDMAX

510bh

27h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.IDMAX

6232

1858

Unsigned32

Read Only

-

AXIS2.MOTOR.IDMAX

71768

1185

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.IDMAX

6232

Float

Read Only

-